Create scan classes

TIP:
You must have administrator privileges to create scan classes.
To create a scan class
  1. Click
    Manage Points
    , and then click
    Edit Scan Class(es)
    .
  2. At the bottom of the page, click
    New
    .
    The new consecutive name of the scan class appears in the
    Scan Point
    box.
  3. At the top of the page, in the
    Time
    text box, type a time value in seconds.
  4. Click
    Save
    .
  5. Click
    OK
    to close the dialog box, and then click
    Restart
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal