Manage shortcuts

Shortcuts are user-defined names for connections with controllers located in a local or remote chassis. A shortcut additionally contains the CIP path to a controller in a chassis.
You can use shortcuts to:
  • Assign meaningful names to controller connections.
  • Search for data points in the Add Points Wizard and on the
    Add Individual Points
    page.
In FactoryTalk Historian ME, you can perform the following actions on shortcuts:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal