(optional) Install FactoryTalk Historian SE patch

If you want to integrate your
FactoryTalk Historian ME
with
FactoryTalk Historian SE
2.1, you need to install the
FactoryTalk Historian SE
patch. Once installed,
FactoryTalk Historian ME
can work with
FactoryTalk Historian SE
to collect, store, analyze, and visualize data using reporting tools such as time-series trends, bar charts, pie charts, pareto, and tabular trends.
The
FactoryTalk Historian SE
patch must be installed on the
FactoryTalk Directory
and any other computer that will be administering the
FactoryTalk Historian ME
module through the
FactoryTalk Administration Console
.
The patch is not necessary for machines with
FactoryTalk Historian SE
2.2 or newer.
You can download the
FactoryTalk Historian SE
patch from the
Rockwell Automation
Knowledgebase page
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal