Upload files to the module

To upload a file to the FactoryTalk Historian ME Module
  1. Click the
    Advanced
    tab, and then click
    Upload Management
    .
    The
    Upload Management
    page appears.
  2. In the
    File Type
    list, select the file type.
    For details on the file types you can select, see File types.
  3. In the
    Please Select File
    box, type the file name, or click
    Browse
    to locate the file.
    The file name may only contain the following characters:
    @, ., -, _, a-z, A-Z, 0-9
    , and must not contain any spaces.
  4. Click
    Upload To Module
    to upload the selected file to the module.
    The uploaded file is displayed in the table. The table includes the name, type, and size of the file, as well as the time the file was last modified.
    TIP:
    Files of type
    Ca Certificate
    ,
    Server Certificate
    , and
    Private Key
    must have the
    .pem
    extension. Files of type
    AutoDiscoveryRuleFile
    ,
    TagAttributeFile
    , and
    User-defined Timeouts
    must have the
    .xml
    extension.
    The maximum size of the file you want to upload may not exceed 500 KB.
    If you use HTTPS, do not delete files of type
    CA Certificate
    ,
    Server Certificate
    , and
    Private Key
    after uploading them.
    For details on security settings, see Manage security.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal