Create users

To create a user
  1. Click the
    Configure Historian
    tab, and then click
    User Management
    .
    The
    User Management
    page appears.
  2. Click
    New
    .
    The
    Create User
    page appears.
  3. In the
    User Name
    box, type the user name.
    The user name must be any combination of lowercase and uppercase characters (a-z, A-Z) and digits (0-9).
  4. (optional) In the
    Description
    box, type a description.
  5. In the
    Password
    box, type the user password.
    The password must be any combination of lowercase and uppercase characters (a-z, A-Z) and digits (0-9).
  6. In the
    Confirm Password
    box, confirm the password.
  7. (optional) In the
    Groups
    box, select the groups that you want the user to belong to. For details, see View groups.
  8. Click
    Save
    to create the user.
  9. Click
    Back
    to return to the
    User Management
    page.
    The newly created user is displayed in the user list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal