Set the time zone

To set the time zone
  1. Click the
    Advanced
    tab, and then click
    Time Management
    .
    The
    Time Management
    page appears.
    The current time zone is displayed under
    Time Zone Setting
    .
    The default time zone is
    US/Eastern
    (Eastern Standard Time).
  2. In the
    Region
    list, select the region.
  3. In the
    Time Zone
    list, select the time zone.
  4. Click
    Save
    .
    TIP:
    Time zone settings for the module affect the time displayed on the
    Home
    page and on the system log message timestamps.
    Event timestamps receive the time zone settings from the client.
    If you have moved your module to a different time zone, updating only the time will not automatically update the time zone in the module information. To have the correct time after the reboot of the module, you need to update both the time zone and the time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal