System status

The
System Status
section displays the following information:This item | Displays |
|---|---|
Point Server | FactoryTalk Historian ME server that manages the archives and provides access to historical data. The status may be Running or Error. |
Data Collection Service | FactoryTalk Historian ME data collection subsystem. The status may be Running, Stopped, or Error. |
Data Transfer Service | FactoryTalk Historian ME data transfer subsystem. The status may be Running, Stopped, or Error. |
Provide Feedback