Module information

The
Module Information
section displays the following information:This item | Displays |
|---|---|
Name | The name of the module. To change your module name, click the Advanced tab, and then click System Settings .For details on the module name and information on the impact of changing the module name, see Change the module name. |
Firmware Version | The version of the firmware. |
Current Time | The current time of the module. To configure time settings, click the Advanced tab, and then click Time Management . |
Up Time | The total time the module has been running. |
Module Slot Location | The location of the module in a slot in the ControlLogix chassis. |
Serial Number | The serial number of the module. This number cannot be changed. |
Provide Feedback