Refresh views

You can refresh the content of the search results table either manually or automatically.
To refresh the search results table manually
  • Click
    Search
    .
To refresh the search results table automatically
  • Below the table, in the
    Auto Refresh
    box, type a refresh interval in seconds.
When using the
Auto Refresh
option, note the following:
  • It is recommended that you turn off the option if you do not need it.
  • Display the minimum amount of data necessary to reduce memory consumption.
  • Choose the refresh rate prudently. The faster the auto-refresh frequency is, the more memory it consumes.
  • Turn the auto refresh option off before closing the web browser or opening another page to release the memory that was being used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal