Home

Home
The
Home
tab displays the following information:
Item
Description
Device Name
The name of FactoryTalk Historian ME.
Device Description
The version number of FactoryTalk Historian ME.
Device Location
The physical slot location of the FactoryTalk Historian ME module in the chassis.
Ethernet Address (MAC)
The MAC address of the Ethernet port.
IP Address
The IP address of FactoryTalk Historian ME.
Production Revision
The revision number of FactoryTalk Historian ME.
Firmware Version
The version number of the firmware.
Serial Number
The serial number of FactoryTalk Historian ME.
Up Time
The amount of CPU time used.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal