EtherNet/IP

The
EtherNet/IP
page contains the following sections:
  • Network Settings
    This section displays the following information:
    Item
    Description
    Link Status
    Indicates if FactoryTalk Historian ME is connected to the Ethernet network.
    IP Address
    The FactoryTalk Historian ME IP address.
    Ethernet Access (MAC)
    The FactoryTalk Historian ME MAC address.
    IP Configuration Mode
    Indicates the network setting used for the FactoryTalk Historian ME module.
  • Network Statistics
    This section displays the following information:
    Item
    Description
    Sent Packets
    The number of network packets sent per second.
    Received Packets
    The number of network packets received per second.
    Sent Bytes
    The number of bytes sent per second.
    Received Bytes
    The number of bytes received per second.
    Sent Packets Count
    The cumulative number of total network packets sent.
    Received Packets Count
    The cumulative number of total network packets received.
    Ethernet/IP
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal