Display LED
The
Display LED
page displays the current message being displayed or scrolled on the module LED in further detail and the LED statistics.The page lists
Current Display
and LED Statistics
information. Data for either the static or the scroll display will be available. If a static message is available, there is no scrolling display. If a message is scrolling in the module LED, no static message is available.Item | Description |
|---|---|
LED Static Display | The current message being displayed on module LED. |
LED Scroll Display | The current message being scrolled on module LED. |
The Display LED page lists the Application LED State information under
LED Statistics
. Values include:Item | Description |
|---|---|
Solid green | Indicates that both data collection and data transfer are active. |
Flashing green | Indicates that the data collection is active but the data transfer is not configured. |
Solid red | Indicates that the data collection is inactive. |
Flashing red | Indicates that the data collection is active but the data transfer is inactive. |

Provide Feedback