Web configuration server

The
Web Configuration Server
page lists the following information:
Item
Description
Process Name
The title of the process.
CPU Usage
The percent of CPU utilization.
Memory Used
The amount of memory (in megabytes) utilized by the web configuration server.
Up Time
The amount of CPU time used.
Priority
Indicates the precedence order for the process.
Nice Value
A value that indicates the CPU process priority. The default value is zero. A high Nice value indicates a lower priority for the process. Negative Nice values are a higher priority.
Web configuration server
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal