Overview

The
Overview
page displays the following information:
Item
Description
Component Status
Displays the current status of all firmware components, either Running or Stopped.
Security Mode
Displays the current security mode, either FactoryTalk Historian ME Local Security or FactoryTalk Directory Security.
Last Backup
Displays status, date, file name, and file size of the last backup.
Top Processes
Displays the running processes in descending order based on CPU usage.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal