Startup log
The
Startup Log
page lists log recorded each time the module is rebooted.To search the startup log
- In theTimetext box, type the time parameters.
- In theSourcetext box, type the source you want to search for.
- In theMessagetext box, type the type of message you want to search for.
- In theCounttext box, type the maximum number of records you want the search to return.
- ClickSearch. The selected records appear in the list on the Startup Log page.TIP:For details on time options, see Set start and end times.
Provide Feedback