Data transfer
The
Data Transfer
page lists the following information:Item | Description |
|---|---|
Process Name | The title of the process. |
CPU Usage | The percent of CPU utilization. |
Memory Used | The amount of memory (in megabytes) utilized by the data transfer service. |
Up Time | The amount of CPU time used. |
Priority | Indicates the precedence order for the process. |
Nice Value | A value that indicates the CPU process priority. The default value is zero. A high Nice value indicates a lower priority for the process. Negative Nice values are a higher priority. |
Transfer Rate | Current transfer rate from the data transfer service in events per minute. |
Successful Attempt Rate | The number of attempts to transfer data to the FactoryTalk Historian SE or PI server per hour. |

Provide Feedback