Data storage

The
Data Storage
page displays storage-related information.
The page displays the following information:
Item
Description
Process Information
Contains the process name, CPU usage, memory used, up time, priority, and Nice value.
Archive Storage Information
Displays total archive space, the amount used, and the amount of archive storage space available.
Archive Information
Displays the total number of archive files, the number of transferred files, the total available files, and the archive file size.
Archive Usage Threshold Configuration Information
Displays the percent level at which a warning is triggered and when the archive reaches a critical size. The monitoring frequency refers to how often the archive is scanned for size limits.
Data storage
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal