Data collection

The
Data Collection
page displays the data collection process name, CPU usage, memory used, up time, priority, Nice value, and collection rate.
The page lists the following information:
Item
Description
Process Name
A label for the process.
CPU Usage
The percent of CPU utilization.
Memory Used
The amount of memory (in megabytes) utilized by the data collection service.
Up Time
The amount of CPU time used.
Priority
Indicates the precedence order for the process.
Nice Value
A value that indicates the CPU process priority. The default value is zero. A high Nice value indicates a lower priority for the process. Negative Nice values are a higher priority.
Collection Rate
The current collection rate from the data collection service in events per minute.
Data collection
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal