Start the data transfer
To start the data transfer
- Click theConfigure Historiantab, and then clickData Transfer.
- UnderData Transfer Parameters, clickStart.The status changes fromStoppedtoRunning.If the FactoryTalk Historian SE or PI server becomes unavailable, the data will continue to be stored on the module. When the server becomes available again, it will automatically reconnect, and the data transfer will continue.
Provide Feedback