Remove points from data transfer

To remove points from the data transfer
  1. Click the
    Configure Historian
    tab, and then click
    Data Transfer Points
    .
  2. Under
    Data Transfer Points
    , type the search criteria, and then click
    Search
    .
    The search results are displayed in the table.
  3. Clear the checkbox next to each data point that you want to remove from the data transfer.
    If you want to remove all the data points listed, clear the
    All/None
    checkbox at the bottom of the table.
  4. Click
    Save
    .
  5. Click
    OK
    .
    The outcome of the operation is indicated with a message displayed at the top of the page:
    INFO: Save operation successful.
    TIP:
    This way you only remove the data points from the data transfer service. If you want to remove the data points from the FactoryTalk Historian SE or PI server (for example, in order to free some licenses), you must delete the points on the FactoryTalk Historian SE or PI server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal