Check the data transfer status in the system log

To check the data transfer status
  1. Click the
    Advanced
    tab, and then click
    System Log
    .
  2. In the
    Time
    boxes, set the time range in which you want to view the messages.
  3. In the
    Source
    box, type
    DataTransfer
    , and then click
    Search
    .
    The search results table is populated with messages related to the data transfer.
For details on the system log, see Use the system log.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal