Add points to the data transfer

To add points to the data transfer
  1. Click the
    Configure Historian
    tab, and then click
    Data Transfer Points
    .
  2. Under
    Data Transfer Points
    , type the search criteria, and then click
    Search
    .
    The search results are displayed in the table.
    The table lists all points that fit the search criteria, with the following information:
    Item
    Description
    Selected
    A checkbox that indicates whether a data point has been added to the data transfer.
    Name
    The name of the data point in FactoryTalk Historian ME.
    Type
    The type of the data point.
    Source
    The source of the data point.
    Created in SE/PI Server
    • Y
      - indicates a data point that has already been transferred to the FactoryTalk Historian SE or PI server.
    • N
      - indicates a data point that has not been transferred to the FactoryTalk Historian SE or PI server yet.
  3. Select the checkbox next to each data point that you want to add to the data transfer.
    If you want to add all the data points listed, select the
    All/None
    checkbox at the bottom of the table.
  4. Click
    Save
    .
  5. Click
    OK
    .
    The outcome of the operation is indicated with a message displayed at the top of the page:
    INFO: Save operation successful.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal