Install the module in the chassis

FactoryTalk Historian ME has the following product number: 1756-HIST2G.
To install the module, follow the
FactoryTalk Historian Machine Edition Module Installation Instructions (Publication 1756-IN106)
.
FactoryTalk Historian ME receives data from the ControlLogix data collection interface and stores it locally in the module. The module data and system information can be viewed and managed through the FactoryTalk Historian ME webpage.
After you install the module, you can log on to the FactoryTalk Historian ME webpage. See Log on to FactoryTalk Historian ME for details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal