Insert trends in a Microsoft Excel workbook
To insert a trend in a Microsoft Excel workbook
TIP:
The following steps may vary depending on your version of Microsoft Excel.
- Open Microsoft Excel.
- Select the cell in which you want the trend chart to appear.
- Click thePI DataLinktab.TIP:For details, see the prerequisites in Create trends with the FactoryTalk Historian DataLink Add-in.
- In theTag Functionsgroup, clickInsert Trend.TheTrend Add-in Wizarddialog box appears.
- On theDefine the Tracespage, clickData from PI.
- In theServer namebox, type the IP address of your module, or select a module from the list.
- Next to theTag namebox, click
.TheTag Searchdialog box appears. - In thePI Serverbox, select the server on which you want to search the tags for your trend.
- Specify the other filtering criteria, and then clickSearch.The table below the search boxes is populated with the search results.
- Select the name of the tag for your trend, and then clickOK.The selected tag appears in the right pane of theDefine the Tracespage.
- Select the checkbox next to the tag name, and then clickNext.TheSpecify the time rangepage appears.
- In theStart TimeandEnd Timecheckboxes, set the time range from which the data will be displayed.The default value forStart Timeis*-8h.The default value forEnd Timeis*(the current time).
- Select theEnable updatescheckbox, and then clickNext.
- In theTrend title (optional)box, type a name for your trend.
- ClickFormat.ThePI Trend Control Propertiesdialog box appears.
- Select theVertical Scaleproperty.
- On theOptionstab, underScale:
- In theFormatlist, selectGeneral.
- In thePositionlist, selectOutside Left.
- ClickOK.
- In theTrend Add-in Wizardwindow, clickFinish.The trend chart appears in your Excel spreadsheet.
Provide Feedback