Define the server connection
Before you begin using an Excel Add-in, you need to configure a connection to each FactoryTalk Historian ME and FactoryTalk Historian SE server that you are going to use with the Add-in.
To define a server connection to FactoryTalk Historian SE or FactoryTalk Historian ME
- Go toStart > Programs > Rockwell Software > FactoryTalk Historian SE > FactoryTalk Historian SE System > About PI-SDK.ThePI SDK Utilitywindow appears.
- On theConnectionsmenu, clickAdd server.TheAdd PI Serverdialog box appears.
- In theNetwork Path/FQDNbox, type the IP address of your FactoryTalk Historian SE or FactoryTalk Historian ME.
- ClickOK.The server is added to the server list.
- Select the checkbox next to the server.The connection details appear in the right pane of thePI SDK Utilitywindow.The connection status appears at the bottom of the window.
- Repeat the steps for each server that you are going to use with the Add-in.
Provide Feedback