View the data storage information
TIP:
You must have administrator privileges to modify the data storage information.
The data storage service in FactoryTalk Historian ME monitors the NAND flash-based storage used in the module.
To view the data storage information
- Click theConfigure Historiantab, and then clickData Storage.TheData Storagepage appears.
- Review the following for additional information.
Use this section | To |
|---|---|
Archive Statistics | View the information on the current usage of the disk space allocated to the archive. |
Archive Information | View the following information on the archive:
|
Event Queue | View the number of temporary files in a transient state. The module processes the files as soon as it archives events in the files. Usually, the event queue count should be less than 3. Note: When the count gets bigger, it may cause the archive disk to reach its threshold. In such case, the data collection will be automatically stopped, and data interruption will occur.You may set a warning level for the archive disk usage in the Archive Disk Threshold Configuration box to help prevent this situation. |
Log Threshold Configuration | Set a threshold for the log files disk usage. The default setting is 95%. When the log storage reaches its threshold, FactoryTalk Historian ME deletes older log files and logs the following message on the System Log page:<Log file name and path> has been removed because the /mnt/log partition is full. |
Archive Disk Threshold Configuration | Set a threshold for the archive disk usage. The default setting is 95%. When the archive disk reaches its threshold, FactoryTalk Historian ME performs the following actions:
|
Active Usage Threshold Configuration | Set a warning and critical thresholds for the data disk usage, with the following default settings:
|
Provide Feedback