Start and stop the data collection

TIP:
You must have administrator privileges to start and stop the data collection.
To start the data collection
  1. Click the
    Configure Historian
    tab.
    The
    Data Collection
    page appears.
  2. Click
    Start
    .
To stop the data collection
  1. Click the
    Configure Historian
    tab.
    The
    Data Collection
    page appears.
  2. Click
    Stop
    .
    Make sure that that data collection is fully stopped before you start it again.
    TIP:
    You can also start and stop the data collection using:
    • Controller programming languages (the Ladder logic).
    • FactoryTalk Historian ME Logix Designer Module Profile.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal