Set the time zone
To set the time zone
- Click theAdvancedtab, and then clickTime Management.TheTime Managementpage appears.The current time zone is displayed underTime Zone Setting.The default time zone isUS/Eastern(Eastern Standard Time).
- In theRegionlist, select the region.
- In theTime Zonelist, select the time zone.
- ClickSave.TIP:Time zone settings for the module affect the time displayed on theHomepage and on the system log message timestamps.Event timestamps receive the time zone settings from the client.If you have moved your module to a different time zone, updating only the time will not automatically update the time zone in the module information. To have the correct time after the reboot of the module, you need to update both the time zone and the time.
Provide Feedback