Reboot the module

To reboot the module
  1. Click the
    Advanced
    tab, and then click
    Module Shutdown
    .
  2. Under
    Module Reboot
    , click
    Module Reboot
    .
    A message appears asking you to confirm the action.
  3. Click
    OK
    .
    TIP:
    Alternatively, you can reboot the module using the FactoryTalk Historian ME Logix Designer Module Profile.
    If the Restore Defaults or Reset Security actions are being executed on your Historian module in the Logix Designer Module Profile, you will not be able to restore the default settings, reset the security configuration, or reboot the module from the web client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal