Restore
    Use the 
    
    
Restore
 option to return a project to a committed state.
          
     TIP: 
    The 
Restore
 option only removes local commits.
          To use the Restore option:
- SelectFile > Source control > Change history.
- In theChange historytab, select the commit you want to restore.
- SelectRestoreon the top right of theChange historytab.
- In theRestoredialog, selectRestoreto return to the selected project state orCancelto stop the restore action. SelectingRestorecauses all local commits after the restored commit to be permanently removed.
     IMPORTANT: 
    
- A restore will trigger a pull when remote changes are available. If conflicts are detected, theManage conflictsdialog opens. Resolve and accept all conflicts to finish the merge and complete the restore. SelectingCancelwhile theManage conflictsdialog is open also stops the restore action.
- When restoring more than one local commit, all commits are grouped together into one merge.
Provide Feedback