Add and assign devices
    To add devices
:- To add devices to a parent device, right-click the Ethernet Bus or Backplane and selectAdd device.
- Use theCategory filterto select the device categories that you want to add to the project.
- Select the catalog number and useDevices to addsection on the right to increase the number of that device to add to the project.TIP: When the Ethernet Bus or Backplane is full, there will be no available devices to select. You can modify the allocation of devices by adjusting the number of devices added to the project or using the trash can to delete devices.
- SelectContinue. TheAssign devices to projectwindow opens with the selected devices listed in thePending to configurearea.
- Configure each of the devices in thePending to configurelist. When all the required fields for each device are configured properly, theFinishbutton becomes enabled.
- SelectFinishto add the devices to the Ethernet Bus or the Backplane.
To assign devices
:- To assign devices to a parent device, right-click the Ethernet Bus or Backplane of the parent device and selectAdd device. TheAssign devices toparent device dialog box opens.Catalogis the default selection.TIP: The catalog grid shows only compatible devices for the Ethernet Bus or Backplane.
- Select devices to assign to the Ethernet Bus or Backplane. TheDevices to assignlist shows the number of slots or addresses that are available.
- SelectProjectto select a device from the project to assign to the Ethernet Bus or Backplane. The selected device shows in theDevices to assignlist and the number of slots or addresses that are available.
- SelectContinueto assign the selected devices to the Ethernet Bus or Backplane.
- The devices added fromProjectare read-only. SelectFinishto complete the device assignments.
Provide Feedback