Ladder Diagram Properties pane
    Use the 
Properties 
pane in the Ladder Editor to change parameters for the open routine. If Properties
 is not open when you select the ladder diagram routine,  select 
Provide Feedback