Move a ladder diagram rung
    Move a ladder diagram rung to have the instructions on the rung execute at a different time in the routine. 
Prerequisites
To move a ladder diagram rung
Use one of these options to move a ladder diagram rung:
- In the ladder diagram, drag the rung selection region of the rung to a valid drop zone. Valid drop zones are indicated by .
            TIP: To move a rung, right-click the rung header and then select eitherMove rung uporMove rung down. Valid drop zones may vary from rung to rung. Dropping the ladder element in its original location does not move or copy the element. .
            TIP: To move a rung, right-click the rung header and then select eitherMove rung uporMove rung down. Valid drop zones may vary from rung to rung. Dropping the ladder element in its original location does not move or copy the element.
- To cut or copy and paste a rung, right-click a rung and selectCutorCopy. Select the rung above which you want to paste the rung. Right click and selectPaste.
Provide Feedback