Edit a ladder diagram rung
    Edit a rung in a ladder diagram to change the functionality of the rung in the routine. A routine must be available to edit (not read-only) to edit a ladder diagram rung.
Prerequisites
To edit a ladder diagram rung
        - Add, remove, or change the order of instructions on a rung by:- Right-clicking the instruction to cut, copy, paste, or delete the instruction or add an element to the instruction.
- Moving the instruction by dragging and dropping it to a new location.
- Using theToolboxto add a new instruction.
 
- Change the tags that are referenced or used as operands by double-clicking the tag name to type a new name or selecting the down arrow to open the Data Item Browser to choose a name.
- Add branches to a rung by selecting the branch in theToolboxand dragging the branch onto the rung.
Provide Feedback