Delete a rung comment
    Delete a rung comment to no longer describe the tasks that the rung performs in the routine.
Prerequisites
To delete a rung comment
Use one of these options to delete a rung comment. With both options, the message 
The rung comment was deleted
shows after the delete action is complete.- Right-click the rung and selectDelete rung comment.
- Right-click the rung, selectEdit rung comment. In theRung commentdialog, selectDelete.
Provide Feedback