Toggle a BIT instruction
    Toggle the state of a Boolean tag for a BIT instruction. If the parameter is ON, toggle the instruction to turn OFF the parameter. If the parameter is OFF, toggle the instruction to turn ON the parameter. 
Prerequisites
- Add a BIT instruction to a rung. You cannot toggle an OSR or OSF instruction.
- Add a Boolean tag to the instruction.
To toggle a BIT instruction
- In the instruction, select the operand.
- From the menu bar, selectFile > Edit Ladder Diagram > Toggle Bit.
Provide Feedback