Delete a ladder diagram instruction
    Delete a ladder diagram instruction to remove the instruction from the rung or branch in the routine.
Prerequisites
To delete a ladder diagram instruction
- In the ladder diagram, select the instruction or instructions to delete and then pressDelete.TIP: To delete an instruction, you can right-click the instruction and then selectDelete.
Provide Feedback