View and open MCC lineup documentation
    You can access MCC lineup documentation that was imported into a FactoryTalk Design Studio project. You can view MCC lineup drawings, manuals, and spare parts, if applicable  
Prerequisites
- At least one MCC lineup documentation has been imported into FactoryTalk Design Studio.
To view and open MCC lineup documentation
:- In theElevationview, right-click a selection.
- Select one of these options:- Documentation > Drawingsto view a list of drawings associated with the MCC lineup. The drawings are identified by file name, sheet number, path, and if it is a custom drawing. Double-click a drawing to download it to your local drive.
- Documentation > Manualsto view a list of manuals associated with the MCC lineup. The manuals are identified by file name, publication description, publication date, path, and if it is user supplied. Double-click a manual to download it to your local drive.
- Documentation > Sparesto view a list of spare parts associated with the MCC lineup. The spare parts are identified by part number, part description, quantity required, quantity recommended on hand, category, and provides four blank columns to uniquely customize the identity of the spare part once you order the part.
 Access drawings, manuals, and spare parts from the section level, unit level, or a lineup level. Right-click a section, unit, or the white space outside a lineup to access documentation from these three areas
Provide Feedback