Unit Profile
    Use a Unit Profile to view detailed information about the selected unit, including:
      
- a list of devices contained in the unit.
- a summary of device information.
- the current device status, if enabled.
- links to documentation and device profiles.
Launch the Unit Profile in either the IntelliCENTER explorer or in the Elevation view.
Provide Feedback