Replace units
    Use the 
Replace unit
 option to exchange an empty door with a Units-only dataset.Prerequisites
        - Purchase and download the dataset folder.
- Unzip the dataset folder to your local drive.
- AFactoryTalk Design Studioproject with lineups.
- In theElevationview, right-click on an empty door and selectReplace unit.
- In theReplace Unitdialog box, selectBrowseunderDatabase.
- SelectImport.The empty Door is replaced with the imported unit-only dataset.
Provide Feedback