Import Sections
    Use the 
Import Sections
 option to add sections to existing lineups. Prerequisites
        - Purchase and download the dataset folder.
- Unzip the dataset folder to your local drive.
- A FactoryTalk Design Studio project with lineups.
To add sections to an existing lineup:
- From the IntelliCENTER MCC lineup explorer tree, right-click and selectImport Sections. TheImport Sectionsdialog box opens.- To add new sections, selectBrowseunderDatabasesto locate the Sections documentation. The import tool reads the dataset and shows a list of available lineups.
- To replace a door or existing unit, selectBrowseunderDatabasesto locate the replacement Unit documentation.
 
- Select one or more lineup and selectImport.
Provide Feedback