Import an MCC lineup
    Import MCC lineups from datasets purchased with IntelliCENTER MCCs documentation associated with it (post-shipment) or without documentation associated with it (pre-shipment).
Prerequisites
- Purchase and download the dataset folder.
- Unzip the dataset folder to your local drive.
To import an MCC lineup
In FactoryTalk Design Studio:
- Open or create a project.
- SelectFile > Import > MCC lineupto open theImport MCC Lineupdialog box.- To import an MCCs dataset, underDatabases, selectBrowseto locate the dataset folder on your local drive.
- To import MCCs lineup documentation, underDocumentation, selectBrowseto locate the folder on your local drive.TIP: You have the option to browse for both databases and documentation and add them to the lineup in one import step.
 
- Select one or more of the lineups and selectUploadto import the datafiles into FactoryTalk Design Studio.
Provide Feedback