Allocate FactoryTalk Smart Object or program to a controller and task
    Allocate an existing 
FactoryTalk Smart Object
 or program to a controller or task. - In the explorer bar, select System. System.
- Select theFactoryTalk Smart Objector program.TIP:Properties > Sizeshows how large the Smart Object or program is.Sizeis stated in blocks of memory and is the sum of all the programs belonging to the Smart Object.
- InProperties, select theAllocationtab and select:- Controller. Select a controller from the list to allocate the program ofFactoryTalk Smart Objectto a controller.- SelectNoneto leave the program orFactoryTalk Smart Objectunassigned.
 
- Task. Select a task from the list to allocate the controller to a task.- SelectNoneto leave the controller unassigned
 
 
Provide Feedback