Enable FactoryTalk Remote Access for FactoryTalk Design Studio
     You can configure communication between FactoryTalk Remote Access and FactoryTalk Design Studio by creating and configuring the FactoryTalk Remote Access 
FTDS
 user. 
     NOTE: 
    To work together, the instances of FactoryTalk Remote Access and FactoryTalk Design Studio you are using must be entitled within the same organization in FactoryTalk Hub. FactoryTalk Design Studio can only communicate with the FactoryTalk Remote Access instance in the same FactoryTalk Hub organization. See Entitlements in the FactoryTalk Remote Access Online Help
This task requires you to have entitlements allocated for using FactoryTalk Remote Access.
- To enable the FTDS user in FactoryTalk Remote Access for use with FactoryTalk Design Studio:
- Open the FactoryTalk Remote Access application in FactoryTalk Hub.
- On the left side of the screen expandSettingsby selecting the down arrow.
- SelectDomain Options, theOptionsscreen appears.
- Select theEnable FactoryTalk Design Studio (Linx) integrationbox and selectSave.Selecting this option creates a FactoryTalk Remote Access user labeledFTDSwhich you will use to set permissions.
- SelectExplorer > Domain Viewon the left side of the screen.
- Select the device or folder with the endpoints that you want to connect via FactoryTalk Design Studio. You can connect to a single endpoint or set permissions for all the endpoints you have placed in a folder for your organization.FactoryTalk Remote Access endpoint devices enable secure connectivity to your controllers. Granting endpoint access to the FTDS user enables FactoryTalk Design Studio to communicate through the endpoint to on-premises controllers. To deploy to an on-premise controller with FactoryTalk Design Studio, the controller must be accessible on the same network as a FactoryTalk Remote Access endpoint device.For more information on how to add an endpoint device, see:FactoryTalk Remote Access Manager Toolsin the FactoryTalk Remote Access Help. For this step look at the help forDevice Registration to Domain.
- Select the endpoint to which you want to assign permissions for the enabledFTDSuser. An information panel opens on the right side of the screen.
- Select the arrow next toPermissionsto expand the permissions list.
- Select the plus sign next toPermissionsto add the FactoryTalk Design Studio user.
- Select the plus sign next to the user labeledFTDSto add the user then close theAdd Permissionsdialog by selecting the x at the top right of the box. TheFTDSuser now appears in the Permissions list.
- Select theFTDSuser.
- UnderPermissions Operationsselect the arrow to expandInteractive Access.
- Select theAllowbox next toNetwork Access (VPN). TheFTDSuser now has permission to access the selected endpoint device. To give theFTDSuser permission to all endpoint devices in the organization, highlight the top level in your folder structure and repeat this process
FactoryTalk Design Studio can now use the 
FTDS 
 user to communicate with devices connected to FactoryTalk Remote Access endpoints. Next you must configure the endpoints in FactoryTalk Design Studio. Go to Connect FactoryTalk Design Studio to FactoryTalk Remote AccessProvide Feedback