Open a project
    - Close any open project.
- To open a project, either:- On theWelcomepage, selectOpen project.
- On theWelcomepage, select a project from theRecent projectslist.
- From the menu bar, selectFile > Open project.
 
- InOpen project, inOpen from, select the location of the project:- Local. Open a project from your local workspace.
- Remote. Open a project from the shared repository.
 
- Select the project to open.
- SelectOpen.TIP: You cannot open a project from the shared repository when it already exists in your local workspace. Open the local project.
Provide Feedback