Import a Logix Designer project
    Use the
 Import Logix Designer project
 option to bring a Logix Designer L5X project into FactoryTalk Design Studio.
     TIP: 
    If you refresh or close the browser while the import process is being executed, some imported content might show on the 
Execution
 explorer, but you will not be able to download the log files from FactoryTalk Design Studio.To import a Logix Designer project:
- SelectFile > Import > Logix Designer projectto open theImport Logix Designer projectdialog box.
- SelectBrowseand search for the Logix Designer L5X project to import into FactoryTalk Design Studio. You can import only a complete L5X project file that is no larger than 500 MB.
- Select an L5X file to import into your FactoryTalk Design Studio project and then selectImport. Partial L5X exports and L5X file names with special characters are not supported.- After a successful import, you will see anImport modificationsmessage. Content from the L5X file may have been renamed, updated, or removed during the import. Download the Log file to see more information about the modifications made during the import process. The log file will appear in yourDownloadsfolder, where it can be viewed in a text editor.
- If you see theProblem during importmessage with aDownload the log fileoption, it means the import executed but it was not successful. For more information about the imported L5X project, selectDownload the Log fileto yourDownloadsfolder.
- If you see theProblem during importmessage with aRetryoption, it means the import did not execute. SelectRetryimport to import the L5X file again.
 
Provide Feedback