Close a project
    Close a project when changes are complete or close a project in order to open another project.
        
- On the menu bar, selectFile > Close project.TIP: If autosave is in progress, "Saving" appears in the title bar next to the project name.
Provide Feedback