View tabs
    In 
FactoryTalk Design Studio
, tabs open for certain functionality, including the Tag Editor, routines for the Ladder Editor, and Change history
. You can open a tab for every routine in a ladder diagram, making it harder to navigate the open tabs. Use the Window 
menu to select which tabs to view and close.  - In the menu bar, selectWindowand then select:- Next tab. View the next open tab.
- Previous tab. View the previously open tab.
- Close tab. Close the current tab.
- Close all tabs. Close all open tabs.
- All tabs. View a list of open tabs to select the tab to view.
 
Provide Feedback