View messages and status with the Output pane
    Output 
displays a Console
 tab and a Messages
 tab.- TheMessagestab displays warning, warning, error, and error, and information messages. Messages appear for either the entire project or the current open tab in FactoryTalk Design Studio. Enter a term inSearchto display related messages or scroll to view message descriptions and the associated locations in the ladder diagram. information messages. Messages appear for either the entire project or the current open tab in FactoryTalk Design Studio. Enter a term inSearchto display related messages or scroll to view message descriptions and the associated locations in the ladder diagram.
- TheConsoletab displays controller deployment and connection statuses.
Select  
 
 
 Output
 to open the pane.Provide Feedback