System explorer
    Use the 
System 
explorer to focus on the logical design of your project. Create FactoryTalk Smart Object elements to create tags, programs, and routines. The logic in the FactoryTalk Smart Objects defines the behavior of an item in a system or a plant. Reuse FactoryTalk Smart Objects by adding them to the 
Library 
explorer for modeling a system or plant. For example, create a FactoryTalk Smart Object for a tank in a large plant. You can then reuse the same FactoryTalk Smart Objects for all tanks in the system instead of creating logic for each tank. Complete the design of the system and then allocate the FactoryTalk Smart Objects to a controller in the Execution 
explorer. Online, offline, and mixed state indicators
      When you go online with a controller, additional status indicators appear in the 
System 
explorer. These indicators can appear next to a FactoryTalk Smart Object or any of its elements. - Green rails appear next to the programs that are allocated and deployed to the online controller. Green rails also appear next to any Smart Object that is related to the program.
- The offline only indicator appears if an element is allocated to the online controller but has not been deployed. appears if an element is allocated to the online controller but has not been deployed.
- The online only indicator appears if an element is deployed to the online controller but is not present in the offline project. appears if an element is deployed to the online controller but is not present in the offline project.
- If no green rail illuminates and there are no online only or offline only indicators, then either:- The element is not allocated.
- The element is allocated to a controller that is different than the online controller.
 
- A mixed state icon appears next to the parent components when the child components have differences in online-only, offline-only, or green rail allocation states. See Mixed state scenariofor a sample user mixed state user scenario. Expand the child nodes to see differences in states and allocations. appears next to the parent components when the child components have differences in online-only, offline-only, or green rail allocation states. See Mixed state scenariofor a sample user mixed state user scenario. Expand the child nodes to see differences in states and allocations.- In this example, a green rail appears next to FactoryTalk Smart Object SO1 and its child programs Prg1_AllocatedC1 and Prg2_AllocatedC1 to indicate they are online and executing. The green rail does not appear next to Prg3_AllocatedC2 and Prg4_unallocated because they are not online and not executing with the current online controller.
  
     TIP: 
    Online and offline only indicators appear based on how elements are named. When a green rail is present but no icon appears, a component with this name exists offline and has been deployed to the controller. There may be differences between the online and offline components, such as different tags or ladder logic. 
     TIP: 
    Some menu commands are not available for elements that are online only. These commands are disabled.  
     TIP: 
    When moving elements that exist online and offline, the old location displays the online-only icon and the new location displays the offline-only icon.
     TIP: 
    Renaming an element that exists online and offline causes the component to appear twice in the tree. The old name appears next to the online-only icon. The new appears next to an offline-only icon. 
Overview of status icons
      The System explorer displays status icons in the tree that represent when a task or program is inhibited and when a component has multiple conditions online or offline.
- The icons are displayed in priority order:- Online- Major Fault
- Minor Fault
- Inhibit Status
- Validation Errors
- Warnings
- Information Messages
 
- Offline- Inhibit Status
- Validation Errors
- Warnings
- Information Messages
 
 
- Each icon has a tooltip that provides details of the status of the component, task or program. If the inhibit state is cleared, the icon will be replaced by the next icon in the priority order.
- When a component has multiple conditions online or offline, an icon tooltip provides details with each status showing first online status and then offline status in priority order. If the status changes, the icon will be replaced by the next status in priority order and the tooltip will update.
Provide Feedback